The King Edmund School | Hager UK

The King Edmund School

We worked with Gainsborough Electrical contractors to install an energy monitoring solution at King Edmund School in Essex that will enable detailed reporting and manage energy consumption. 

King Edmund School

The King Edmund School | Energy Monitoring

Our energy monitoring solution panelboard installed in King Edmund School in Essex provided detailed reporting and increased energy efficiency. 


Phase one of the major refurbishment involved the installation of our 800A rated panelboard with meters fitted to all outgoing circuits at the school. We worked with Gainsborough Electrical contractors to install an energy monitoring solution at King Edmund School in Essex that will enable detailed reporting and manage energy consumption. 

 
Phase one of the major refurbishment involved the removal of old switchgear and installation of our 800A rated energy monitoring panelboard with meters fitted to all outgoing circuits at the school, which took just two weeks during the holidays to minimise disruption.


"The Hager panelboard and meters proved simple and fast to fit."

Alan Hawes, Managing Director at Gainsborough Electrical 


With the incoming cable entering through the ceiling, phase two of the installation proved even more complex. To avoid bending and stressing the cable and affecting its termination into the Panelboard, we supplied an engineered solution with the incomer repositioned at the top of the panelboard. 

The detailed metering goes beyond the requirements of Part L and is part of the school’s policy to record and manage its long term energy consumption. Providing protection and monitoring for half of the school, the 800A rated Panelboard allows for possible future expansion of the electrical load. Additionally, plans include a new IT suite and an extension of air conditioning to more rooms. 

Alan Hawes, managing director at Gainsborough Electrical comments: “The school has expanded rapidly over the years and outgrew its original mains switchgear. The installation was complex for a number of reasons. 

“The Hager panelboard and meters proved simple and fast to fit so that we could meet the school’s specification within a very narrow timeline. Phase two was even more complex and Hager was able to respond with a bespoke engineered solution.”

Stephen Dyson, our market manager, added: “We pride ourselves on being able to respond to customer challenges and this solution was recommended and installed promptly and should have a significant impact on energy consumption and cost savings over the coming years.”


Products used in this case study

Get inspired and discover how you can use our electrical installations in your next project!  

test

Energy Distribution | Hager Panelboard

The invicta 3 panelboard range includes 250A, 400A, 630A & 800A panelboards with MCCB incomers. Prewired meter packs allow installers to fit metering into the board.



Discover
similar case studies

Enjoyed what you read? Below are similar case studies where we were able to provide an ideal solution for a variety of projects! 

test

Flying Start | Hager Building Automation

Using the building automation system, Hager’s electrical solution combines the building’s intruder alarm system with shutters that secure all of the windows and doors. 

test

Grangefield Academy and Manor College

The project encompasseddaylight dimming throughout the installation, reducing energy use further. In the offices, Hager occupancy sensors have also been fitted.

test

Spire Nottingham Hospital | Hager Lighting Connection

The hospital in Nottingham is the latest addition to the 38-strong Spire hospital portfolio and Hager has worked alongside main M&E contractor, Briggs & Forrester and system consultant, Parker Wilson Consulting (PWC) to devise a lighting control system that meets the requirements of the hospital.