Hull prison | Hager UK

Hull Prison

Our IP65 rated GRP en­clos­ures were able to provide an ideal fix with minimal disruption to Hull Prison cells. The tailored solutions team developed a spe­cial­ised con­sumer unit to provide cir­cuit pro­tec­tion for Hull Prison cells.

Hull Prison

Hull Prison | En­ergy Dis­tri­bu­tion 

Our IP65 rated GRP en­clos­ures were able to provide an ideal fix with min­imal dis­rup­tion to Hull Prison cells. Our Tailored Solu­tions team de­ve­loped a spe­cial­ised con­sumer unit to cir­cuit pro­tec­tion for Hull Prison cells.

Our Tailored­ Solu­tions team de­ve­loped a spe­cial­ised con­sumer unit to provide cir­cuit pro­tec­tion for Hull Prison cells. In ad­di­tion, the board had to fit into a small foot­print and be fast to in­stall to min­im­ise dis­rup­tion to staff and in­mates. The con­sumer units for the cells are of­ten housed in riser cup­boards that also con­tain wa­ter pipes and cisterns. The pre­vi­ous metal units had star­ted to cor­rode and needed re­pla­cing.

 

With pro­tec­tion against wa­ter in­gress a pri­or­ity, we sup­plied its solu­tion with IP65 rated GRP en­clos­ures. In ad­di­tion, the board had to fit into a small foot­print and be fast to in­stall to min­im­ise dis­rup­tion to staff and in­mates. Each con­sumer unit is split into two pan as­sem­blies to provide sep­ar­ate RCD and MCB pro­tec­tion for two cells. Both as­sem­blies within the board also have an in­dic­ator light so that staff can quickly check that there is power sup­plied to the cells without need­ing to enter.

To speed up in­stall­a­tion we as­sembled the boards with the devices in the fact­ory. The boards are daisy-chained to­gether and can be sup­plied with IP rated plugs and sock­ets to fur­ther speed up the in­stall­a­tion. Our Tailored Solu­tions is a ser­vice that can provide an ex­act product that meets the needs of a par­tic­u­lar in­stall­a­tion, which is not avail­able off the shelf. Cus­tom­er’s have the peace of mind of fact­ory as­sured qual­ity to ISO 9001:2008.



Products used in this case study

Get inspired and discover how you can use our electrical solutions in your next project.

test

IP65 GRP Enclosures

Orion enclosures are available in steel or GRP material finish, in a range of sizes to suit any installation.

 
test
 
test
test
 


Discover
similar case studies

Enjoyed what you read? Check out some more of our other case studies to see how we were able to provide an ideal electrical solution.  
test

The King Edmund School | Hager Energy Monitoring

Leading electrical solutions and services provider, Hager, has worked with Gainsborough Electrical contractors to install an energy monitoring solution at King Edmund School in Essex that will enable detailed reporting and manage energy consumption. 

test

Aberdeen City Campus | Hager Lighting Connection System

Hager was chosen thanks to its ease of installation, flexible use, reliability and cost effectiveness and is now providing enhanced lighting control system for both the theatre users and onsite lighting maintenance staff.

test

Flying Start | Hager Energy Distribution

Using the building automation system, Hager’s electrical solution combines the building’s intruder alarm system with shutters that secure all of the windows and doors.