Updated Guidance on RCCB Testing

Guid­ance for Test­ing 
CD285U RCCB


Devices pro­duced up to July 2019

 ** Please note: This guid­ance DOES NOT ap­ply to CD285U RCCB with a pro­duc­tion date code after 19219 **


The new range of Hager Type A RCCBs con­form to BS EN 61008-1 Amended 2017.  This stand­ard re­cog­nises RCCBs not ex­ceed­ing 30 mA as provid­ing ad­di­tional pro­tec­tion against elec­tric shock.

 

Table 1 of BS EN 61008-1 spe­ci­fies the man­u­fac­turer’s op­tion of a max­imum break time (com­monly re­ferred to as trip­ping) for a 30 mA RCCB as 40 ms at a test cur­rent of 250 mA.  This is aligned to IEC TS 60479 which relates to the ef­fects of elec­tric cur­rent on hu­mans and which re­cog­nises 250 mA dis­con­nect­ing within 40 ms.  This was re­flec­ted in the 18th edi­tion BS 7671 in the note un­der 643.8 which states:

 

Ef­fect­ive­ness is deemed to have been veri­fied where an RCD meet­ing the re­quire­ments of Reg­u­la­tion 415.1.1 dis­con­nects within 40 ms when tested at a cur­rent equal to or higher than five times its rated re­sid­ual op­er­at­ing cur­rent.

 

Un­for­tu­nately, the ac­cept­able test para­meter of a max­imum trip time of 40 ms at  250 mA  has not yet been trans­ferred to in­dustry guid­ance  which still de­scribes a single test op­tion i.e. dis­con­nect within 40 ms at 5IΔn and is there­fore still the re­cog­nised prac­tice in the UK.

 

Test Readings

The product stand­ard BS EN 61008-1 al­lows the man­u­fac­turer to se­lect char­ac­ter­ist­ics of 5xI∆n or 0.25 A / 250 mA. The Hager RCCB is set to 0.25 A / 250 mA which al­lows con­form­ity to both the product stand­ard and BS 7671.

 

Test Procedure

Mar­ket feed­back in­dic­ates that there may be a gen­eral is­sue around how to cor­rectly test 30 mA RCCBs set to 0.25 A.

 

Reg­u­la­tion 643.8 re­quires the veri­fic­a­tion to be made by visual in­spec­tion and test­ing.  The test could be car­ried out us­ing either the ‘Auto’ func­tion of the in­stall­a­tion test meter or manu­ally se­lect­ing each test in turn.  We re­com­mend the RCCB test is car­ried out in ‘manual mode’.  The test should be car­ried out at the device it­self with all loads dis­con­nec­ted, as de­scribed in IET Guid­ance Note 3 and IET On-Site-Guide. 

 

The test equip­ment should be se­lec­ted to the type of RCCB cor­res­pond­ing to the type of RCCB within the in­stall­a­tion.

 

Should you wish to carry out a test at 250mA, where the re­quired dis­con­nec­tion time is within 40 ms, a vari­able RCCB test in­stru­ment can be set to 50 mA and tested at X5, which is in ef­fect car­ry­ing out the test at 250 mA, as per­mit­ted by the note un­der Reg­u­la­tion 643.8.

 

Also should your par­tic­u­lar test in­stru­ment not have a vari­able fa­cil­ity then it is ac­cept­able to carry out the test at a higher value of 300mA (set ma­chine to 300mA and x1) to achieve a time within 40ms.

 

The 1x test is no longer a re­quire­ment but could of course be car­ried out.  The ac­cep­ted re­quire­ments for this test are for dis­con­nec­tion within 300 ms as stated within IET Guid­ance Note 3 and IET On-Site-Guide.

 

Further Support

We are fully com­mit­ted to sup­port­ing our cus­tom­ers and should you re­quire any fur­ther cla­ri­fic­a­tion or sup­port please con­tact our Hager Tech­nical Sup­port line on 01952 675689.


Author: Paul Collins, Technical and Training Manager

 

More from the 18th Edition

Surge Protection

A transient overvoltage or surge is a short duration increase in voltage measured between two or more conductors. In short this means anything from microseconds (millionths of a second) to a few milliseconds (thousandths of a second) in duration.

Read more

 

Selection of RCD Types

RCD's exist in various different forms and react differently depending on the presence of DC components or different frequencies.

Read more

 

Overload Protection

Devices such as switches, RCCBs etc. in distribution boards and consumer units may have historically had their rated current determined after having taken diversity into account but without having considered overload protection of the devices.

Read more

 

BEAMA Guides

A collection of the latest guides relating to 18th Edition, Hager is proud to be a technical contributor to these guides which provide technical advice on a range of 18th Edition related topics.

Read more