Surge protection reality check | Hager UK

Surge Protection
Reality Check


Hager Gets Real On Surge Protection

According to recent industry research, surge protection remains the number one area of concern for electrical contractors following the introduction of the 18th Edition of the Wiring Regulations.

 

A poll by Hager highlighted almost one in three contractors admitted to still being unsure about their responsibilities around surge protection, with selecting appropriate solutions for both residential and commercial installations the biggest area of confusion.

 

To provide an at-a-glance overview to help contractors better understand their responsibilities to remain compliant, Hager has produced a Reality Check graphic guide, which is available to download below the article.

 

The Reality Check sets out the key points to consider when thinking about where surge protection devices should be fitted on commercial installation projects, and outlines the range of potential overvoltage scenarios contractors need to be mindful of. It also highlights instances where risk assessments should be undertaken, as well as offering practical guidance about approaching residential applications. To help electrical contractors, Hager provides a pre-fitted distribution board which includes a surge protection device built-in, removing the need for additional wiring.

 

The Reality Check is part of a range of helpful support material Hager has produced for electrical contractors to help them better understand the 18th Edition of the Wiring Regulations. These include bespoke 18th Edition training courses held at Hager’s purpose-built training academy at Telford.

 

Updated on 29/07/2019


 

More from the 18th Edition

Surge Protection

A transient overvoltage or surge is a short duration increase in voltage measured between two or more conductors. In short this means anything from microseconds (millionths of a second) to a few milliseconds (thousandths of a second) in duration.

Read more

 

Selection of RCD Types

RCD's exist in various different forms and react differently depending on the presence of DC components or different frequencies.

Read more

 

Overload Protection

Devices such as switches, RCCBs etc. in distribution boards and consumer units may have historically had their rated current determined after having taken diversity into account but without having considered overload protection of the devices.

Read more

 

BEAMA Guides

A collection of the latest guides relating to 18th Edition, Hager is proud to be a technical contributor to these guides which provide technical advice on a range of 18th Edition related topics.

Read more