Dumfries Photovoltaics

Dumfries contractor JB McCormick has used our circuit protection and control for the installation of photovoltaic (PV) panels on 19 public buildings.

Dumfries Photovoltics

Dumfries Photovoltaic  | Circuit Protection 

Dumfries and Galloway Council’s investment in solar PV are to reduce its carbon footprint and energy costs in line with the Scottish Government targets set out in the climate change (Scotland) 2009 Act.

The contract covers primary schools, secondary schools, ice rinks, swimming pools and other buildings. To date, the council has saved about 500,000kWhr of power and generated 600,000kWhr.

With each installation varying in size, the project manager for JB McCormick, Eric Thomson, selected us because of the company’s modular solution for the control and circuit protection.

We offer various sizes of AC and DC rotary handle switches, a DC1000V din rail rotary switch, a 4 pole type B RCCB, surge protection devices, photovoltaic fuse carriers and fuses and metering. The solutions are housed in different sized enclosures.

Says Chris Wood-Gee, sustainable development team leader for the council: “As long term owners of the buildings, we needed robust and reliable installations. Local company Solway Solar, who won the contract, demonstrated that they had selected high quality equipment for the entire installation including the control and circuit protection supplied by Hager."



Hager products used in this case study

Get inspired and discover how you can use our electrical installations in your next project! 

Invicta TP&N

The invicta 3 panelboard range includes 250A, 400A, 630A & 800A panelboards with MCCB incomers. Prewired meter packs allow installers to fit metering into the board.

test

Surge Protection

Hager Surge Protection Devices (SPDs) protect electrical and electronic equipment against transients, originating from lightning, switching of transformers, lighting and motors.



Discover
Similar case studies

Enjoyed what you read? Below are similar case studies where we provided an ideal solution for a variety of projects! 

test

The King Edmund School | Hager Energy Monitoring

Leading electrical solutions and services provider, Hager, has worked with Gainsborough Electrical contractors to install an energy monitoring solution at King Edmund School in Essex that will enable detailed reporting and manage energy consumption. 

test

Aberdeen City Campus | Hager Lighting Connection Module

Hager’s Klik lighting control module (LCM) solution has been specified at a busy theatre at the Aberdeen City Campus, part of the North East Scotland College.

test

Dundee University | Hager Lighting Connection System

Using Hager's KNX lighting control system, McGills installed a single 30V bus line throughout the library extension, as opposed to a conventional hardwired solution that would have used multiple cables.