Sollysta range enhanced with new Key Switch Socket

Hager’s popular Sollysta wiring accessories range has been further strengthened with the launch of a new White Moulded 13 Amp double pole key switch socket with LED indicator.

 


Hager's Sollysta range enhanced with key switch socket to prevent unauthorised use

 

Hager’s popular Sollysta wiring accessories range has been further strengthened with the launch of a new White Moulded 13 Amp double pole key switch socket with LED indicator.

 

Designed as an ideal switch socket solution for communal area application including multi-residential buildings, hotel lobbies and student accommodation, the integrated fish key switch function ensures that power cannot be turned on or off on the socket without the use of the removable key. This feature prevents unauthorised use.

 

The White Moulded switch socket has clear directional markings for ‘on’ and ‘off’ and offers ease of use through the key operation and the integrated vibrant red neon LED which brightly illuminates when power to the socket is in the ‘on’ status.


"Unauthorised use could lead to faulty appliances being connected to the socket and resulting in short circuiting and tripping. The key switch function can prevent this"

Dogan Dogan

Solution Manager for British Standard at Hager 

As with all switched sockets in the Sollysta range, the new addition offers a double pole construction with both the live and neutral conductors ensuring safe isolation of the plugged-in appliance.

 

An additional benefit for its use in communal areas includes the socket’s manufacture from high quality Urea-Formaldehyde. This provides anti-bacterial and anti-viral properties tested to ISO 22196:2011 to help support the protection of people by reducing potential viral transference through touch. 

 

Dogan Dogan, Solution Manager for British Standard at Hager says: “The integrated double pole key switch socket with LED indicator is the latest addition to the extensive Sollysta range of wiring accessories from Hager. It offers security of and works perfectly as, for example, a cleaner or landlord’s socket ensuring that only authorised personnel can use the socket for safe and tested equipment. Unauthorised use could lead to faulty appliances being connected to the socket and resulting in the inconvenience of short circuiting and tripping. The key switch function can prevent this, making it ideal for use in communal settings.” 

 

Discover the new key switch socket here


Sollysta Wiring Accessories

Designed to be the easiest on the market to install