Financial District, London

Hager’s flexible and innovative Klik lighting connection system has been installed as part of a major refurbishment project for an iconic building in the heart of London’s financial district.

 


Klik lighting connection solution adds up at renowned location in the financial district


Hager’s flexible and innovative Klik Lighting Connection system has been installed as part of a major refurbishment project for an iconic building in the heart of London’s financial district.

 

With its pre-wired plugs, Klik connection helps reduce installation time on site, eliminates the chance of poor connections, and allows for the lighting system at the renowned building to adapt as needs change. It was these benefits, together with Hager’s ability to quickly respond to the customer brief, which has seen the solution specified as part of the ongoing upgrade work taking place within one of the capital’s most iconic buildings.

 

With the initial refurbishment works commencing on Level 6, the main challenge for the lighting requirements of the project was the need for the connection system to link seamlessly with the third-party front-end PC-control system which would control the entire lighting system on the floor.

 

Ben Byram, Klik key account manager from Hager, explains: “After being approached by the project’s consultant, we worked together to quickly devise a lighting connection solution that would easily dovetail with the front-end PC-based lighting control system already selected. 

 

“Using the flexibility that underpins the Klik connection system, we were able to speedily supply a bespoke connection PDF installation plan that the onsite electrical contractors were able to easily follow to support installation. The detailed schematic, which Hager’s expert design team can provide for all commercial projects, ensured the installation of the Klik system was straightforward and delivered tangible time savings for the project.” 

 

"Klik can adapt to meet any requirements"

Jason Pritchard, Project Specification Manager


As the use of the sixth floor of the world famous building accommodates general office space, bathrooms and shower rooms, the Klik connection system was able to incorporate the specific aspects of the Level 6 refurbishment without the requirement for additional connectors and accessories. 


Jason Pritchard, Project Specification Manager at Hger added: “Using the benefits of standard prefabricated wiring systems with a flexible design, Klik can adapt to meet any requirements. The pluggable system ensures no complications will arise with future refurbishments too as lights can be relocated quickly and easily. In addition, Klik’s unique design prevents any unwanted disconnections due to load on cables or vibrations.”


Traditional lighting systems often struggle to adapt when a building or office space needs to change as is the case with the refurbishment project at the heart of London's financial district. With the Klik connection solution, moving to a new layout is as easy as plugging in. Together with the transparent installation plan that was devised by the company’s technical experts without delay, Hager’s Klik connection system and extended service has helped ensure an excellent installation experience for the contractors and project managers. 


It is anticipated that the benefits delivered by the Klik lighting connection solution will also be seen in other parts of the building as the large-scale refurbishment project extends to other floors within the acclaimed site. 

 

Project Information

Building type: Commercial
Project type: Refurbishment
Products used: Klik Lighting Connection


Want to talk to our Hager team about this project?

 

Jason Pritchard

    

 Areas covered: London & Surrounding areas

 

Email: jason.pritchard@hager.com

Mobile: 07979541193


Products used in this
case study

A modern lighting connection & control system

Klik's prefabricated wiring system and adaptable design makes installation a quick and easy process. 

tbd

Klik Marshalling Boxes

Marshalling boxes allow the connection and control of multiple luminaries and come in sizes from 4 to 12 ways.

 

See the range

TBD

Klik Ceiling Roses

7 pole conduit box/surface connector to allow the easy connection of digital lighting within traditional fixed wire installations. 

 

See the range

TBD

Klik Plugs

Connections to the luminaires are made via pre-wired plugs and leads. All leads are factory tested to standard BS 7211. 

 

See the range


Looking for more interesting case studies?