Hager extends Sollysta socket range
Hager has extended its popular Sollysta wiring accessories range, with the introduction of a new White Moulded and Part M USB A+C Twin Switched Socket.
Hager has
extended its popular Sollysta wiring accessories range, with the introduction
of a new White Moulded and Part M USB A+C Twin Switched Socket.
Acknowledging
the continued demand for in-home portable device charging, Hager’s trusted Sollysta
range now includes a double pole twin switched socket that incorporates both a Type
A and the emerging Type C USB port, with the two charging ports capable of delivering
a total charging current of 3.1 Amps.
The
addition of the USB Type C port is an exciting market development, and further
extends the functionality of the Sollysta wiring accessories range.
With USB-C
expected to eventually replace USB Types A and B, and Micro USBs, installing
the new solution will future proof home wiring accessories as USB-C emerges as
the common standard for charging and transferring data. USB-C
ports are currently included in many new portable devices such as laptops, phones,
and tablets. Smaller and thinner than their predecessors, the USB-C connector
can be plugged in either way with no risk of damage.
Intelligent
connection
The
Sollysta 13A Twin Switched Socket with USB A+C ports has built-in intelligent
connection, enabling the socket to identify itself as the dedicated primary
charger for the connected device. This
provides maximum charging capacity and improvements to charging speeds as the
device allows the socket to safely bypass its trickle/safety charging mode.
Like all
options within the Sollysta range, the socket features the patented 3 pin
safety shutter system and the double pole socket that switches both the live
and neutral conductors to ensure safe isolation of the plugged-in device.
The USB-C
function is initially available on the White Moulded and Part M ranges but will
in time be extended across the entire Sollysta portfolio.
"Extending our Sollysta range through offering a Type C USB port, in addition to the Type A port, means the newly created twin switched socket supports the emerging standard for safe and speedy portable electronic device charging."
“As new devices appear on the market, USB-C is set to become the common USB port solution and homes that install the Sollysta twin switched socket with both Type A and Type C USB ports will be ideally placed to benefit from quicker and safer device charging outcomes. The inclusion of intelligent connection functionality, overload protection, as well as the patented 3 pin safety shutter system, makes this an exciting and benefit-led addition to the high performing Sollysta range.”
Sollysta
The full Sollysta range is available in White Moulded, Decorative, Grid, IP66, Part M and Metal-clad options. Electrical contractors can take advantage of the tried and trusted wiring accessories for both residential and commercial projects, which have been designed from the start to be the easiest on the market to install.Advantages of Sollysta
for installers
Across the range
Sollysta was designed from the start to be the easiest on the market to install. We've kept these hallmark
features across the range to ensure that no matter what you're installing, it's always a simple job.