Case Study Cash Back: Terms and Conditions 

This offer is only available to Insight team members who are residents of the United Kingdom aged 18 years or over except employees of Hager Ltd and their close relatives and anyone otherwise connected with the organisation. 

By submitting a project for a case study, the Insight team member is indicating his/her agreement to be bound by these terms and conditions.

 

•This offer starts on [20/1/2021] and will finish on [31/12/21] 

 

•Selection of case studies is at the discretion of Hager Ltd., and shall not be obliged to accept any applications for the Insights Team case study cashback offer. 

•The project submitted for a case study must be completed within 3 months of their submission date for this incentive.   

•The project must take place in a commercial or large residential setting i.e. care homes, student accommodation, office buildings, schools, etc.  

•All parties involved in the project (i.e. the electrical contractor and the facility where the project is taking place) must give consent to publishing a case study around the project. 

• The case study must feature the installation of Hager products.  

•The installer is responsible for providing all the contact information necessary to put the content together for the case study. This involves contact information for individuals involved in the project.   

•Hager will be solely responsible for creating the case study as well as coordinating and paying for a photographer to attend the site.   

•To receive cashback, once the project is complete and live, the installer must provide an invoice displaying Hager products used in the project.   

•50% cash back criteria: The project must be live and complete. If the case study is complete and includes full photography of the products installed and the facility (coordinated by Hager), the installer will receive 50% cash back (up to a max value of £500) towards the Hager kit used for the project.   

•25% cash back criteria: If a case study is completed and access to the site and photos of the installation were unable to be attained, then the installer will receive 25% cash back of the Hager kit used in the project (up to a max value of £500).   

•Cashback will only apply to Hager products shown on the invoice, excluding any other brands utilised in the project.   

•The invoice will be reviewed by Hager and if approved, the cashback will be paid to the installer’s business bank account.   

•Hager Ltd shall have the right, at its sole discretion and at any time, to change or modify these terms and conditions, such change shall be effective immediately and communicated to Insight team members 

•Hager Ltd also reserves the right to cancel the case study cashback offer if circumstances arise outside of its control. 

•By accepting these terms and conditions, Hager Ltd. Have the rights to use case study material in present and future digital and print media marketing campaigns.