KNX Touch Control
The inte­l­li­gent all-rounder

Outstanding design meets comp­re­he­n­sive comfort




Architects

Touch me with proxi­mity sensor

Seduction is an inte­rplay. The new KNX Touch Control makes the start: As soon as the user approaches, an inte­g­rated proxi­mity sensor acti­vates the high-resol­ution 3.5" TFT touch display. At the same time, an addit­i­onal function can be triggered via the corre­s­p­o­nding commun­ic­ation objects. How the game conti­nues is dete­rm­ined by the user - by mane­u­ve­ring his finger over the up to ten pages and calling up to six funct­ions per screen. Since the eye also cont­rols, the display illum­in­ation is autom­at­ic­ally adapted to the room light via an inte­g­rated brig­ht­ness sensor.


Lights on, blinds down, scene starts
Each side can be assi­gned up to six buttons or up to three rockers - depe­nding on the number in a horizontal or vert­ical arran­gement. An overview of all confi­guration options can be found in the instal­lation manual.

Knowing how, knowing how much
In addition to the operating options, the KNX Touch Control can display various energy or tempe­rature values - and thus prom­otes the effic­ient use of energy.


Dim the light or turn up the cooling

For cumu­lative control proc­e­sses, we recom­mend the digital "rotary control", which can be combined with one or two buttons on each side. It gives the user an almost magical feeling when cont­ro­l­ling their house.

Individual touch

Image data for the screen saver or other icons for desi­gning the pages can be uploaded using microSD card.


Recom­me­nded areas of applic­ation

- Offices
- Small comme­rc­ials
- Show­rooms
- Villas

Art of touch - like no other

The new KNX touch control is a room control unit and tempe­rature cont­ro­ller in one and masters the art of touch like no other. With the high-resol­ution touch display, building control becomes a pleasure. 

As the "little black dress on the wall", it antic­ipates your cust­o­mers' every wish from their fing­e­rtips. The inno­vative design blends disc­re­etly into any ambience - from upscale resid­e­ntial buildings to repre­s­e­ntative commercial buildings. Design frames from Berker ensure harmo­n­ious inte­g­ration into the prefe­rred switch range.

Need help? Any question?

Do you have a question, do you want free advice? Feel free to contact us. We're here for you.

Desc­ri­ptive Textarea to enter Text values......Desc­ri­ptive Textarea to enter Text values......