Deniz Istanbul Marina Houses

As part of the Deniz Istanbul deve­l­o­pment project, the Marina Houses now have a special status.

hg_IP_Turkey_Deniz_Marina_Houses01_1080x720


As part of the Deniz Istanbul deve­l­o­pment project, the  Marina Houses now have a special status. There are 87 first-class villas in an area of 64,000 m2 not far from the Sea of Marmara coastline. And every bit as exce­pt­i­onal as the prop­e­rties are the switches and control systems that manage them – both from Berker. 


Project: Villa Quarter
Location: Yakuplu, Istanbul
Arch­itects: Kraft Arch­itecture/Hakan BaÄŸcı & Nazlı Tınastepe
Products & solutions: Berker B.IQ anth­racite control system, Berker K.5 switch range
www.hager.com.tr

Want to know more?