Power surge protection
Keeping people and property safe.
Power surges are the main cause of defects in electronic devices – with claims of over 200 million euros per year. Therefore, power surge protection devices are a must for safe electrical installation: in all buildings, all over the world.
Surge protection
The three types of surge protection devices
Protection technology from a single source
In doing so, we follow the motto: less is more. We have reduced the number of variants and made the portfolio more manageable. Fewer products now cover even more applications.

Combine and reinforce
Current Hager surge protection devices are fully compatible with existing products and can be easily combined in existing projects without any issues.
Level of
protection
Overvoltage arresters protect against
transient overvoltages which may cause the
deterioration of electrical equipment and the
destruction of the electronic components of
the receivers. They can be used in all
earthing systems (neutral point system).

Norm-compliant range
All Hager surge protection devices meet the applicable standards of IEC 62305-3 and IEC 60364-5-53 and are compliant with the lightning protection requirements defined in IEC 62305.
Combine and reinforce
Important for retrofitting: Current Hager surge protection devices are fully compatible with existing products and canbe easily combined in existing projects without any issues....
Commercial building protection
As the energy demand of buildings increases, so do the requirements for surge protection. Analogue to apartment buildings, the VdS guideline “Risk-oriented lightning and surge protection” VdS 2010:2021-02 should be consulted for assistance. This is also relevant for the compliance of functional buildings in reference to the lightning protection class. The requirements set out here apply to the vast majority of functional buildings.

Residential
building protection
Lightning protection is not usually required for single-family homes. This means that often, no external lightning conductor is installed. In this case, only the IEC 60364-4-44 is applicable for protection against sur- ges in this area. As the simplest way to comply with the normative minimums, Hager recommends installing its combi- nation arresters in the mains-side near the service entrance. If the cable length of ten metres is exceeded, for example to the sub-distribution, the standard recommends additional surge arresters Type 2 and 3.

More SPD overvoltage protection
Our brochure gives you a good overview of overvoltages and their causes and effects, the protection concepts in the various applications and the comprehensive solutions from Hager.
Get evolved
Hands-on classes with
experts in their fields.
Have a question?
Our team of technical experts are on hand and ready to answer any questions you may have!