Arc Fault Detection Devices
Increasing Protection
Arc fault protection devices (AFDD) use microprocessors to identify characteristic current flow and voltage curves that indicate an arc fault and automatically trip the affected circuit.
This significantly reduces the risk of fire due to faulty conductors and connections. The protective function of the AFDD has already proven its worth internationally, and has been used in Germany since February 2016.
The 18th edition of BS 7671, when published in July, recommends the use of these to provide additional protection against fire.
Monitoring via Microprocessor
An AFDD is activated by both series and parallel arc faults. Unlike circuit breakers or RCDs, an AFDD does not have an electromechanical trigger, but utilises electronic technology to analyse the signature (waveform) of an arc. It reliably differentiates between an arc fault and the signature (waveform) in normal switching and control events, preventing false tripping.
Potential Causes
- Kink / break in a cable
- Cable wear due to frequent use
- Cable damage resulting from drilling or construction work
- Incorrect wire stripping
- Incorrect bending radii
- Loose screwed connections
- Defective wall plugs
- Rodents biting cables
An AFDD will trip the circuit when a potentially hazardous arc occurs, eliminating the resulting fire hazard.
Ring Final Circuits
Contrary to common belief, AFDD’s do offer protection against arc faults in ring final circuits and to the equipment being fed from this circuit. A series arc fault in one leg however, is unlikely to be at a dangerous level so will not be detected. This is due to current in this instance flowing around the other leg of the ring. A series arc fault will be detected in equipment and in flexible cables connected to the ring final circuit. Parallel arc faults are detected and disconnected in all parts of the ring circuit and on all connected equipment.
FAQs:
What does AFDD stand for?
Arc Fault Detection Device.
Where do I need Arc Fault Detection?
AFDD's should be installed in a location that is easily accessible. They protect 120 volt, single-phase, 15- and 20-ampere branch circuits supplying electrical outlets or devices that are installed in kitchens, living rooms, family rooms, recreation rooms etc.
How does an AFDD work?
AFDD's work by protecting against arc faults when they instantaneously trip a circuit when they detect electric arcs. This prevents the possibility of a fire occurring.
What types of circuits can AFDDs be used on?
The regulations specify that 230 volts ac final circuits that include ring circuits, radials, spurs and more.
Effective Areas Of Protective Devices Depending On Fault Position & Type
Fault Between | Short Circuit | Overload | Residual Current | Serial Arc | Parallel Arc |
L-L | MCB / RCBO | MCB / RCBO | - | - | - |
L-N | MCB / RCBO | MCB / RCBO | - | AFDD | AFDD |
L-PE | MCB / RCBO | MCB / RCBO | RCD / RCBO | - | RCD / RCBO / AFDD |
Further Information
The Hager technical team contribute to a number of key industry publications, for AFDD we have been involved in the preparation of the BEAMA Guide to Arc Fault Detection Devices (AFDDs)
Downloads
Arc Fault Detection Files
Download our documentations below, containing everything you need to know about Arc Fault Detection and the 18th Edition-
At a Glance | Arc Fault Detection
All of the key info you need to know about Arc Fault Detection Devices.
pdf394.79 KB -
Bitesize Guide | 18th Edition
Our small guide to everything you need to know about the 18th edition.
pdf1.3 MB -
Residential Distribution Catalogue
Our Residential Distribution Catalogue contains all of our 18th edition solutions for residential applications.
pdf4.57 MB
More from the 18th Edition
Surge Protection
A transient overvoltage or surge is a short duration increase in voltage measured between two or more conductors. In short this means anything from microseconds (millionths of a second) to a few milliseconds (thousandths of a second) in duration.
Selection of RCD Types
RCD's exist in various different forms and react differently depending on the presence of DC components or different frequencies.
Overload Protection
Devices such as switches, RCCBs etc. in distribution boards and consumer units may have historically had their rated current determined after having taken diversity into account but without having considered overload protection of the devices.
BEAMA Guides
A collection of the latest guides relating to 18th Edition, Hager is proud to be a technical contributor to these guides which provide technical advice on a range of 18th Edition related topics.
Related Products
An AFDD solution tailored for you
Our Arc Fault Detection Devices complying with BS EN 62606 form the basis of our offer. However, when combined with our distribution systems, provide a solution which has been rigorously tested and validated to offer optimum protection against the harmful effects of dangerous electric arcs.