Overload Protection 


Devices such as switches, RCCBs etc. in distribution boards and consumer units may have historically had their rated current determined after having taken diversity into account but without having considered overload protection of the devices.

These devices do not provide protection against overload and the 18th Edition prescribes that overload protection of the switch or RCCB shall not solely be based on the use of diversity factors of the downstream circuits. 


Methods of protection 

We recommend one of the following methods of protection against overload:

Method 1

Ensure the sum of the rated current of the downstream MCBs do not exceed the rated current of the switch or RCCB (Inc). This method would however need to consider the consequences of any spare ways and later additions.

Summary:

A consumer unit with a rated current of 100A (InA), with two RCCB 100A (Inc) will allow the consumer unit to be installed in any single phase application up to 100A


Method 2

Ensure that the rated current of a switch or RCCB (Inc), stated by the assembly manufacturer, is not less than the rating of the upstream OCPD. For a domestic installation this could be a 100A cut-out fuse.

Note

Potential future loads on spare ways should be considered


Method 3

Select a consumer unit or distribution assembly that only utilises RCBOs on outgoing circuits. Consideration will still need to be given as to the rated current of the main switch.


What the Regs say

536.4.3.2
"RCCBs & switches do not provide protection against overload, therefore they shall be protected by an overcurrent protective device."

536.4.202

“ ... overload protection shall not solely be based on the use of diversity factors of the downstream circuits. To achieve overload protection of RCCBs or switches, the rated current of the overcurrent protection device (OCPD) shall be selected according to the manufacturers instructions”.


Downloads

More from the 18th Edition

Surge Protection

A transient overvoltage or surge is a short duration increase in voltage measured between two or more conductors. In short this means anything from microseconds (millionths of a second) to a few milliseconds (thousandths of a second) in duration.

Read more

 

Selection of RCD Types

RCD's exist in various different forms and react differently depending on the presence of DC components or different frequencies.

Read more

 

Arc Fault Detection 

Arc fault protection devices (AFDD) use microprocessors to identify characteristic current flow and voltage curves that indicate an arc fault and automatically trip the affected circuit.

Read more

 

BEAMA Guides

A collection of the latest guides relating to 18th Edition, Hager is proud to be a technical contributor to these guides which provide technical advice on a range of 18th Edition related topics.

Read more


Related Products

Check out our solutions below. 

Design Consumer Units

Our range of Consumer Units includes our metal Design Consumer Units, along with an insulated range for installations that don't need to comply to the latest regulations.

TBD

100A RCCB

Hager Residual Current Circuit Breakers (RCCBs) provide RCD earth leakage protection (protects against electrical shocks by direct or indirect contacts).They open automatically in the event of an earth fault between phase and/or neutral and earth.