Tailored
Solu­tions

We can provide the right solution that meets your specification.

If your en­quiry falls out of the stand­ard of­fer, Tailored Solu­tions can meet your re­quire­ments

 

To dis­cuss your pro­ject needs with our tech­nical ex­perts, call us on 01952 675 689, or use the link be­low to fill out our on­line form.


Hager Engineered Solutions

What are Tailored Solu­tions? 

From fit­ting devices through to be­spoke en­gin­eer­ing, Tailored Solu­tions provides a com­plete ser­vice for any pro­ject.

For your pro­ject, we can of­fer a solu­tion that can meet the most de­mand­ing of chal­lenges. From design & en­gin­eer­ing through to lo­gist­ics, our 

Tailored Solu­tions ser­vice of­fers un­rivaled sup­port & peace of mind for you and your busi­ness.

Design & engineering input at the pre-order stage

Our teams will design and engineer a bespoke solution at an early stage for your project. The teamwork approach ensures that we can accommodate even the most demanding requirement.

Technical support throughout the project life-cycle

Our dedicated Tailored Solutions team are all based on the same site, and are on hand throughout the life-cycle of the project, with expert knowledge and understanding of your requirements.

Factory tested and assembled before despatch

Our rigorous factory testing ensures any tailored solution is fully compliant to the latest regulations and your specification, ensuring minimised risk and total confidence on product performance.

Delivery and call off schedules

We will deliver the solution to you exactly when you need it, directly to site, all at once or piece by piece. We tailor our delivery to suit your needs.

Site specific logistics

For even the most demanding of sites, with specific delivery time slots and access restrictions, our team will make sure the solution is on site when and where you need it.



Arc Fault De­tec­tion 

Extra protection. Extra peace of mind.

The 18th Edi­tion of BS 7671 re­com­mends the use of AF­DDs to provide ad­di­tional pro­tec­tion against fire.

Our Tailored Solu­tions team can help you im­ple­ment AF­DDs in res­id­en­tial or com­mer­cial pro­jects.

AFDD Arcs

Harmful Arcs

Arc Fault Detection Devices provide greater peace of mind to building owners and operators by protecting the building and its occupants from electrical fires caused by electric arcing. The technology allows the protection device to identify the signature of a harmful electric arc and disconnect the supply before a fire can start.

AFDD Solution

Our AFDD offer

Our Arc Fault Detection Devices complying with BS EN 62606 form the basis of our offer. However, when combined with our distribution systems, provide a solution which has been rigorously tested and validated to offer optimum protection against the harmful effects of dangerous electric arcs. Hager devices are a two module combined AFDD/MCB, with a comprehensive range.

Multi-residential Solution

When designing electrical installations you need to follow BS 7671:2018 in conjunction with the specification and with a solution that you can be confident in. Our Arc Fault Detection Devices and enclosure systems ensure that where specified you can meet the requirements of BS 7671:2018 and be confident in a proven, safe solution which is easy to install.




Popular Examples

We offer a variety of services to suit your project needs

Surge protection fitted

With renewed emphasis on requirements for surge protection and extra guidance on cable size and length when installing. Factory installing the Surge Protection prior to shipping guarantees the performance of the equipment.

Arc fault detection fitted

We can pre-fit Arc Fault Detection Devices into boards for any project to reduce complexity, to ensure correct configuration is supplied and tested before it arrives on site. We fit AFDDs into both commercial distribution and residential distribution boards.

Metering

To support energy saving requirements on any project, metering is essential. By assembling the CTs, Fuses, Cable Harnesses and Meters with the distribution board, the equipment arrives pre-installed, connected and factory tested.

Panelboard linking

Making the energy distribution work for the specific site requirements is easy, we can link standard distribution boards and deliver a solution that is configured to the correct footprint and layout and pre-programmed ready for use.

Switch fuses

There is often a need for uninterrupted power in buildings for fire alarm systems, emergency lifts or sprinkler systems. We can fit a switch fuse to the live side of the incoming device, with all cabling within the enclosure, to facilitate this.

Dual supply with changeover switch

Occasionally a building will need two power supplies, with a manual changeover switch to control the two. We also provided this board with fuse protection on both supplies and a permanent supply to a sprinkler system regardless of which supply was in use.


Services 

We have a variety of services we offer to accompany our tailored solutions. 

Engineered solutions

Double Marking

Each electrical connection is made to the correct torque setting and indelibly marked by the operator. This is then double checked by a colleague and marked for a second time. The initials of both parties are recorded on the test label. This gives you absolute confidence that all connections are robust. 

Custom Labelling

Labelling of internal cabling and identification of circuits helps ensure the easiest / fastest installation. Additionally, we have plastic or traffolyte labelling available.

Cabling

All internal cabling completed by Hager has cable identification markers and cable management as standard, giving a neat cable solution coupled with easy identification of conductors for the installation and maintenance of the board.


Power and lighting board

The requirement for metering in distribution boards is becoming increasingly common with the lighting and power loads needing to be separately monitored. In addition to our standard range of power and lighting boards we have created a number of bespoke solutions.   

Hager power and lighting board

Bespoke Steelwork

Due to our UK-based manufacturing and design capabilities we are able to provide alterations to steel work to suit the requirements of your project. 

Electrical engineered solution

Pre-assembled Enclosures 

Your distribution board can be supplied with all outgoing devices, blanks, meters, surge protection etc. factory fitted. 

Pre-assembled Enclosures

Fuse Combination Switches 

Fuse Combination Switches give an option to provide a permanent supply to essential circuits even when the main board is isolated. Connected to the incoming side of the main switch the FCS allows the dedicated circuit to be controlled independently of the main board.

Electrical tailored solutions

Testing & Validation 

Tested, veri­fied and com­pli­ant. 

Every tailored solu­tion from us comes as a tested as­sembly to the rel­ev­ant part of BS EN 61439. With each tailored solu­tion, we take re­spons­ib­il­ity for the design, veri­fic­a­tion and the EU de­clar­a­tion of con­form­ity 

Testing and validation

Shipping

Tested and can ship directly to your site   

We can ship your tailored solu­tion dir­ectly to you, re­mov­ing the ex­tra load­ing and un­load­ing through the whole­saler. Our solu­tions are fully built and tested be­fore be­ing shipped, tak­ing into ac­count the ship­ping re­quire­ments, as well as how the board will be trans­por­ted to site. Large linked en­clos­ures can be split onto sep­ar­ate pal­lets to make trans­port­a­tion onsite easier. 


shipping

customer support

Have a question? 

To dis­cuss your pro­ject needs with our tech­nical ex­perts, call us on 01952 675 689, or use the link be­low to fill out our on­line form.


Have some questions?

Check out our FAQ section to answer some questions you may have.


  • How does the pre-order stage, design and engineering part of the Tailored Solutions service work? 

    At Hager, our Tailored Solutions service emphasizes precision and customization. In the pre-order stage, we discuss and understand your project needs in depth. Our designers then craft a solution tailored to those requirements. After finalising the design, our engineering team brings it to life, ensuring efficiency, durability, and safety. Throughout, Hager collaborates closely with you to deliver solutions that align with your project's unique demands.
  • Can you explain the role of the Tailored Solutions team in providing technical support throughout the project life-cycle?

    Hager's Tailored Solutions team is dedicated to ensuring that your project receives the utmost support from conception to completion. From the initial stages, they dive deep into understanding your specific requirements, offering guidance on the best products and configurations for your needs. As the project progresses, they provide timely technical advice to address any challenges or changes that arise, ensuring that solutions are both efficient and compliant. The team's involvement doesn't just end once the product is delivered; they are committed to assisting with installation and post-installation queries. With Hager's Tailored Solutions team by your side, you can be confident of a smooth and well-supported project journey.
  • How does the rigorous factory testing process ensure compliance with regulations and specifications for tailored solutions?

    At Hager, ensuring our Tailored Solutions meet regulations and specifications is of paramount importance. Our rigorous factory testing process begins by meticulously evaluating each custom solution against set benchmarks. This ensures that every component adheres to industry standards and our own stringent quality checks. Through methodical testing, we ensure not only functionality but also safety, durability, and reliability. Any deviations are promptly addressed, and the product undergoes re-testing until it achieves full compliance. Additionally, us at Hager continuously update our testing methodologies in line with evolving regulations and technological advancements. When you choose a Hager Tailored Solution, you're getting a product that has been put through its paces, ensuring it's up to both your standards and ours.

  • How can the tailored solutions team create bespoke products to suit specific needs of a project?

    At Hager, the Tailored Solutions team thrives on adapting to unique project requirements. When faced with a specific need, we begin by closely collaborating with the client to fully understand their specifications and desired outcomes. Drawing on our extensive expertise, we design a prototype that encapsulates these needs. Utilizing state-of-the-art tools and drawing from our vast product portfolio, we ensure that the bespoke product aligns seamlessly with the project's objectives. After a design is settled upon, our dedicated engineering team refines and optimizes it, ensuring it's efficient, compliant, and of the highest quality. The beauty of working with Hager is our agility and commitment. We don't just provide off-the-shelf solutions; we craft unique products that truly resonate with a project's vision and requirements.
  • How does the Tailored Solutions team ensure timely and accurate delivery, especially for projects with challenging site conditions and restrictions?

    At Hager, our Tailored Solutions team understands the intricacies of diverse projects, especially those with challenging site conditions and restrictions. To ensure timely and accurate delivery:

     

    • Thorough Assessment: Before embarking on any project, we conduct a comprehensive analysis of the site's requirements and challenges. This allows us to anticipate potential obstacles and plan for them.
    • Collaborative Approach: We work closely with all stakeholders, ensuring everyone is aligned with the project's goals and timelines. This collaboration ensures that any unforeseen challenges are promptly addressed.
    • Dedicated Project Managers: Every tailored project is assigned a dedicated manager who monitors the delivery process, ensuring that all components arrive on site as per the schedule.
    • Flexible Logistics: Our logistics team is adaptable, allowing us to adjust to any last-minute changes or requirements that may arise due to site conditions.
    • Regular Communication: We maintain open channels of communication with our clients throughout the project. This ensures that you're always updated on progress and any necessary adjustments.

     

    By adopting this proactive and integrated approach, Hager ensures that even the most challenging projects receive their tailored solutions promptly and accurately.