TADO Decomission
-
Why is the Tado integration being removed from domovea?
Tado has recently changed its API policy and now is charging for access. Maintaining this integration would result in ongoing costs that are not feasible given the number of affected Tado users we have.
-
When will the integration stop working?
1st August 2025.
-
How me, as a user will be affected?
Your domovea installation will continue to work
The Tado devices in domovea app will stop working
All sequences and domogram linked with Tado will be affected
Setting up new sequences and domograms with TADO device will be affected. You will not be able to add trigger and action on a Tado device. -
Are there any other thermostats in domovea which can be used? Workaround?
No workaround for Tado is present at the moment. Though, you can continue to use your TADO installation with native Tado app. You can download the app from the app stores.
-
Which all features in domovea will be affected?
All features linked to Tado device:
- New Tado device cannot be added
- Existing Tado devices will stop to function
- Setting up new domogrammes & sequences where Tado devices are involved (trigger, action..)
- Existing sequences and domogrammes -
Will the integraton work locally?
No, the integration won't work locally too.
-
Will the integration with other IOT devices like IFTTT, Alexa will also be effected?
Yes, the integration with other IOT devices like Alexa and IFTTT will stop to work if it is linked to a TADO device.
-
I have a domovea V3 reference (TJAS471 & TJAS671). Will I also be affected?
Thanks to matter feature on domovea V3 reference, you can make a bridge between your Tado X reference and domovea devices. This way, you can control your Tado X device via matter controller.
Please note:
Tado X reference can only be controlled if you have a matter controller (google home, amazon alexa or apple home)
Only Tado X references are currently supported by matter bridge functionality in domovea.